Two-Factor authentication

Two-factor authentication (2FA) is a very secure way to protect access to your account. It requires you to identify yourself using two different factors, when accessing the domain. The second factor is related to a personal device. You can think of the two factors as something you know (your password) and something you have (your smartphone).
The two-factor authentication consists of a set of credentials (username and password) and a code (or token). The code is a unique number that is generated through a dedicated App and is constantly changing.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal