OptixPanel
graphic terminals

OptixPanel
Graphic Terminals integrate both FactoryTalk Optix and FactoryTalk Remote Access Runtime. Terminals are available in two configurations:
  • OptixPanel
    Standard Graphic Terminal
    : It is provided with a Pro Runtime entitlement.
  • OptixPanel
    Compact Graphic Terminal
    : It is provided with a Basic Runtime entitlement and allows to purchase an entitlement upgrade.
NOTE: See Entitlements for more information about this subject.
NOTE: For further information on the OptixPanel
Graphic Terminals, see the documentation provided at the link https://www.rockwellautomation.com/en-us/products/hardware/allen-bradley/new/optixpanel-graphic-terminals.html
The image below shows the the
FT Optix
section in System Manager.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal