Entitlements
Entitlements allow HMIs or IPCs to be connected to with FactoryTalk Remote Access and determine the operations that are granted by that connection.
There are two main types of entitlements for using FactoryTalk Remote Access:
- FactoryTalk Remote Access Runtime entitlement:This Runtime entitlement can be a Pro or Basic entitlement, featuring an initial 90-day trial period coming with two Pro Trial entitlements.
- FactoryTalk Remote Access 1/2/5/10/25/50 Concurrent Connection entitlement:This domain entitlement comes with an initial 90-days trial period and may be purchased in volumes of 1/2/5/10/25/50 concurrent connections.
Entitlements for both domains and devices in your organization are shown in the
Entitlements
section in the FactoryTalk Remote Access Manager. In this area, you can see how many entitlements allocated to devices have been assigned and how many are still available to you.See the following table for more information:
FactoryTalk Remote Access Runtime Basic | Basic entitlements allow file transfers, task management, and minimal VPN capabilities.
NOTE:
OptixPanel Compact graphic terminals display an
Upgrade button next to the Basic entitlement type, in the right pane of the Domain view , in the Entitlements section. This button allows you to upgrade the Basic entitlement to more advanced types by purchasing just the services that are not already included in the Basic entitlement. |
FactoryTalk Remote Access Runtime Pro | Pro entitlements allow VPN access to all devices on the computer network, file transfers and task management. |
FactoryTalk Remote Access Runtime Pro Trial | The FactoryTalk Remote Access Runtime Pro entitlement allows full use of the Pro entitlement features. |
FactoryTalk Remote Access 1/2/5/10/25/50 Concurrent Connections | Domain entitlements are acquired through the FactoryTalk Hub and determine how many concurrent connections you can establish at the same time. |
NOTE:
See How to activate a entitlement to learn how to activate an entitlement.
Trial Period and first organization creation
When creating your first organization in the FactoryTalk Hub, your domain will be associated with a 90-day free trial entitlement. During this time, you will be required to purchase an entitlement lasting 365 days starting from its activation date. Nevertheless, if you wish to create another organization, you must already have an entitlement associated with your first organization. Then you must purchase entitlements for any more organizations.
Besides the entitlement purchased for each further organization, a 90-day free trial entitlement will be associated with your domain anyway. The free trial entitlement allows for an indefinite number of concurrent connections.
- Access your organization in FactorytalkHub.com.NOTE: See FactoryTalk Remote Access Manager Authentication for further information on this topic.
- Click the FactoryTalk Remote Access tile. If you are accessing FactoryTalk Remote Access for the first time, a window message will prompt you to name your new FactoryTalk Remote Access domain.
- You will be redirected to the FactoryTalk Remote Access Manager and the entitlement trial period starts.
Entitlement expiration
When an entitlement expires, the domain connected to it expires too.
- FactortyTalk Remote Access Runtime Trial entitlementsexpire after 90 days and no grace period follows the entitlement trial expiration.NOTE: Notification messages will appear each time you log on to the service informing you of the number of days remaining in the trial period. After the trial period is over, you will not be able to use the service until you obtain a subscription.
- FactoryTalk Remote Access 1/2/5/10/25/50 Concurrent Connection entitlementsexpire after 365 days and a 7-days grace period following the expiration date activates to allow for entitlement renewal through the FactoryTalk Hub. If the entitlement is not renewed within the grace period, the user can still access the domain, without being able to carry out any action within it.Select theentry to allow each admin and owner user to receive an email every day during the grace period, informing them about any days left to the entitlement expiration.NOTE: 60, 30, and 10 days before theFactoryTalk Remote Access 1/2/5/10/25/50 Concurrent Connection entitlementexpires, an email is sent to all of the admin and owner users to inform them about the expiration deadline.
Features comparison
Features | Runtime Basic | Runtime Pro | Stratix® 4300 Router | OptixPanel™ Compact (Ships with Runtime Basic, Upgradable to Pro) | OptixPanel™ Standard (Ships with Runtime Pro) | Embedded Edge Computer (Ships with Runtime Pro) |
---|---|---|---|---|---|---|
| ✔ | ✔ | x | ✔ | ✔ | ✔ |
| ✔ | ✔ | ✔ | ✔ | ✔ | ✔ |
| x | ✔ | ✔ | x | ✔ | ✔ |
| x | x | ✔ | x | x | x |
Provide Feedback