Duplicate a zone
Copy and paste a zone to duplicate the zone with its properties.
- From the navigation bar, select eitherCanvasorZones.TIP: InZONES, selectOverviewto see all zones in a table.
- Right-click a zone and selectCopy.TIP: Changing between different views does not discard the copied item.
- Right-click blank area and selectPaste.
Add devices to the zone. See Devices.
Provide Feedback