Create a variable type

Create a variable type in
Project view
. You can then create variables of the variable type.
  • From
    Project view
    , drag an existing variable into a folder in
    Type view
    .
    The variable type appears in both
    Type view
    and in the
    Project view
    folder that has the same name as the folder in
    Type view
    .
    TIP: The variable in
    Project view
    is appended with
    (type)
    and the original variable that you dragged from
    Project view
    is now an instance of the type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.