Virtual Meter Dashboard

Provides data from virtual meters, which aggregate information from multiple physical meters. This level allows monitoring and comprehensive analysis of energy usage across various segments, helping to identify trends and implement strategic energy management initiatives.
Click
Virtual meter
from the hierarchy list.
Virtual Meter Dashboard
The following table provides the list of charts available by default in the dashboard:
Chart Types
S.No
Chart Type
Description
1
Trend
The user can view the selected time period with the respective granularity on the X-axis and on the Y-axis, the user can view parameters (Demand). This chart shows the summary of the virtual meter.
2
Bar
The user can view the selected time period with the respective granularity on the X-axis and on the Y-axis, the user can view parameters (Consumption). This chart shows the summary of the virtual meter.
NOTE:
  • When any of the Virtual Meter datalink has issues, the "
    Data loading failed due to data link configuration issues
    " message is displayed.
Related Information
:
Refer to Dashboard Features section to manage the Virtual Meter dashboard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal