Input/Output Instructions

The input/output instructions read or write data to or from the controller or a block of data to or from another device on another network.
Available Instructions
Ladder Diagram and Structured Text
If you want to:
Use this instruction:
Get controller object attributes
GSV
Set controller object attributes
SSV
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal