How electronic signatures work
The steps involved in configuring and executing electronic signatures span the
FactoryTalk Batch
product suite.- TheFactoryTalk Batchsystem administrator sets up electronic signature and signoff security.IMPORTANT:Changing theFactoryTalk DirectoryServer after configuring electronic signatures usingFactoryTalkSecurity is not supported. Doing so may cause Signature Signoffs to fail.
- InFactoryTalk Batch Equipment Editor, theFactoryTalk Event Archiverevent filters for the signature events to capture for use inFactoryTalk Event Archiverwith Reporting Services reports, or other reports.
- Create signature templates for the area model. To obtain electronic signatures for recipe parameters and report parameters of specific phase classes, configure the verification method and signature template to be used when the phase class is created or edited. To download all the limits information to the phase logic, map parameter tags and report tags to the appropriate limit tags on the phases. To require signature verification for the execution of specific commands, set up command verification policies inFactoryTalk Batch Equipment Editorusing the signature templates that were created.
When the master recipe builds, the recipe parameter limits that trigger the verification policy default from the parameter limits specified on the equipment phase. Change these values at the recipe level in
FactoryTalk Batch Recipe Editor
. If configured a phase class to obtain a signature for deviation of report limits, specify those limits on the report for the phase class in FactoryTalk Batch Recipe Editor
. When a batch runs and parameter or report deviations occur requiring signature verification, or the operator issues commands requiring signature verification, a signature is added to the signature list in client, prompting the appropriate users to enter signatures.
FactoryTalk Batch View
, the Electronic Signature HMI Controls, or the e
ProcedureAll signatures record as Signature events in the
FactoryTalk Batch
Event Journal viewer in FactoryTalk Batch View
. Once signature event data generates, create
FactoryTalk Event Archiver
reports, or other reports that capture electronic signature data.This flowchart shows the sequence of tasks in the setup and configuration, execution, viewing, and reporting of electronic signatures:

Provide Feedback