Use the Signature List view
eProcedure
’s Signatures List view allows viewing of all incomplete
signatures associated with currently running batches. Double-clicking a signature opens a
dialog box containing pertinent signoff information about the selected signature.
TIP:
If you are running Internet Explorer version 7.0 or
higher, it is possible to have multiple instances of the
eProcedure
Client
running in the same browser window. The current user will be logged on to all instances.
(See "Running on
internet explorer version 7.x and higher" for more information.)Provide Feedback