Run material-based recipes without the Material Server

If communication is lost with the Material Server, material-based control recipes can continue to process. A highly visible warning message displays when communication is lost with the Material Server. When adding a material-based control recipe to the batch list without access to the Material Server, you must select the materials and containers for binding. For control recipes run without the Material Server, you must update the inventory manually in the Material Editor using the addition and distribution information presented in the Event Journal.
WARNING:
Loss of the Material Server causes the
FactoryTalk Batch
Server to switch to prompt binding and presents an unfiltered list of container/equipment module pairs from which to select binding candidates. The operator must select the container/equipment module pair to supply the correct material to continue processing the batch. Failure to select the correct container/equipment module pair could result in a hazardous situation depending on the material. Exercise extreme caution when operating without the Material Server.
(See the
FactoryTalk Batch
Material Manager
Administrator Guide
for more information about running recipes without the Material Server. See the
Material Editor User Guide
for more information about updating inventory.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal