View material data
If you are running a material-based recipe (MBR), you can view the materials used in each step of the recipe by selecting a step and clicking the
Details
command button.
The following material information is listed on the
Parameter
tab of the Properties
dialog box:- Name
- Low (Minimum)
- Value (Default Value)
- High (Maximum)
- Engineering Units
Once the phase is COMPLETE, you can view the actual amount of material used by selecting a parameter and then clicking the
Details
button. Select the Report
tab to view actual amounts used as shown below:
Provide Feedback