Procedure view command buttons

You can use the Procedure view to command batches that are currently on the Batch List. The Command area includes the command buttons available for the Procedure view. The appropriate command buttons are enabled based on the state and mode of the selected batch.
(See the
Command area
topic for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal