Navigate in the Procedure view

Navigation is the same in both the SFC view and Table view. Double-clicking a step displays the next lower level within the batch. For example, double-clicking a procedure displays the unit procedures for the selected procedure. Double-clicking the initial step displays the next higher level within the batch. Double-clicking the initial step of a unit procedure displays the procedure step. If more than one batch is on the Batch List, you are prompted to select a batch before the Procedure view is opened.
TIP: The initial step is not displayed in the Table view. To display it, double-click outside of the table.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal