SFC view
The SFC view displays the step’s name on the first line, regardless of the level being viewed. Steps that represent unit procedures or operations display their binding information on the second line. If the step is bound, the name of the unit to which it is bound is displayed. If the step is not bound, the alias name is displayed. The step’s current state is displayed in the lower left corner of the step, and the current mode is displayed in the lower right corner of the step. Step or recipe comments generated in the
FactoryTalk Batch
Recipe Editor also display in the eProcedure
SFC view.When a transition is paused,
PAUSED
displays to the left of the transition. When a step is acquiring resources, ACQUIRING1
displays to the left of the transition. All transition expressions display to the right of the transition. The results of the transition expression evaluation can be viewed by double-clicking the transition. The Transition Expression
dialog box opens, displaying the current expression evaluation, or a message stating that the transition expression is not being evaluated..gif/_jcr_content/renditions/original)
A transition in the process of ACQUIRING a phase
Provide Feedback