Information in the Procedure view
The Procedure view includes two separate views of a batch: the Sequential Function Chart (SFC) view and the Table view. The
SFC/Table
command button toggles between the two views. The steps in both views are color-coded, allowing easily recognition of the state of a specific step.
TIP:
If running Internet Explorer version 7.0 or higher, it
is possible to have multiple instances of the
eProcedure
Client running in
the same browser window. The current user will be logged on to all instances. (See
Running on Internet Explorer version 7.x
for more information.)Tip: | If running Internet Explorer version 7.0 or higher, it is possible to have multiple instances of the eProcedure Client running in the same browser window. The current user will be logged on to all instances. (See Running on Internet Explorer version 7.x for more information.) |
Provide Feedback