Equipment view command buttons

Use the Equipment view to command equipment resources and batches that are currently on the Batch List. The Command Area includes the command buttons available for the Equipment view. The appropriate command buttons are enabled, based on the state (and mode, for batches) of the selected resource or batch. (See
Command area
for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal