Navigate in the Equipment view

The Equipment view includes three equipment resource levels: Area, Process Cell, and Unit. The Area level includes icons for each of the defined process cells. The process cell level includes icons for each of the defined units. The unit level includes icons for each of the defined equipment modules.
Double-clicking a resource displays the next lower level. For example, double-clicking a process cell displays all of the units that are included in the selected process cell. You can display the next higher level by double-clicking the background in the Information Area. For example, double-clicking the background while in the unit level displays the process cell in which the unit belongs. If more than one batch is on the Batch List, the process cell level will include a drop-down list of the current batch IDs, listed in order by Create ID. As you navigate down the levels, the information displayed is reflective of the actual state of the equipment, regardless of the batch ID selected in the drop-down list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal