Hyperlinks
Equipment
includes up to five hyperlinks for each process cell, unit, and phase displayed. In the diagram view, view the hyperlinks near the equipment icon. Using the Equipment View Hyperlink feature with
FactoryTalk Batch View
requires changing the location of the files to link to
the appropriate FactoryTalk Batch View
directory.
TIP:
The hyperlink descriptors and defaults are defined in the .
FactoryTalk Batch Equipment Editor
. For more information, see the FactoryTalk Batch Equipment Editor
User GuideTo create a hyperlink folder in the FactoryTalk Batch View
directory
- In File Explorer, navigate to theFactoryTalk Batch Viewweb root directory. IfFactoryTalk Batch Viewis installed in the default location, this is:C:\Program Files (x86)\Rockwell Software\Batch View Server\Bin\wwwroot
- Create a new folder and enter a name for the folder, such asProject_Files.
- Place the files to be linked in this folder.
- InFactoryTalk Batch Equipment Editor, ensure that the path configured for the hyperlink matches the directory path set in step 2 (such as/Project_Files/<file name>).
- Repeat steps 2-4 if using more than one folder for hyperlink files, such asImagesorVideo.
Provide Feedback