Command a batch in the Equipment view

Batch commands may be issued by using the command buttons in the Batch List view, Equipment view and the Procedure view. Only those buttons representing valid commands are enabled. Some of the command buttons are toggles, meaning that depending on the state of the batch, the button label will change. For example, if a batch’s state is READY, the label on the
Start/Restart
button is
Start
. However, if the batch’s state is HELD, the button’s label is
Restart
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal