Labeling Deviations

All new anomalies detected by FactoryTalk Analytics GuardianAI will appear as a deviation. Once a user labels a deviation, it becomes a failure risk until the user marks the anomaly as resolved. The deviation will have associated first principle recommendations. There are several ways to label the deviation:
  • First Principle
    : A user can select from the first principle recommendation, the following image illustrates Cavitation and Viscosity Change.
  • Normal Behavior
    : There might be a case where FactoryTalk Analytics GuardianAI may incorrectly detect the deviation. A user can select normal behavior to train FactoryTalk Analytics GuardianAI to recognize the detected pattern as normal.
  • Other
    : A drop-down will display other labels stored in the FactoryTalk Analytics GuardianAI database from which to select. The user can also choose to create a new label for the deviation.
Deviation Detection and Grouping
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal