Device Definition parameters

Device Definition
includes these parameters:
TIP:
Settings are based on the device being configured. Settings that do not apply to the device are hidden.
Parameter
Description
Device type
Displays the device catalog number and type.
Name
Enter an IEC 61131 compliant device name.
If an invalid character is entered in this field, or if the name exceeds 40 characters, the software ignores the character.
Description
Enter  the description of the device.
Tip
: The description must be within 128 characters. If the description exceeds the maximum length, the software ignores any extra characters.
Slot
Specify the slot number where the device resides. Only slots between 1 and the maximum number of I/O devices are valid depending on the platform.
When the device is created, the slot number defaults to the first available slot position.
When the controller is changed to one supporting a smaller maximum I/O count, the current slot value may no longer be valid.
Series
Specifies the series of the device.
Revision
Specifies the major and minor revisions of the device. The valid range for minor revision is from 1 through 255.
Electronic keying
Defines the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
Valid values include:
  • Exact Match
  • Compatible Module
  • Disable Keying
For detailed information on Electronic keying, see Electronic Keying in
Logix5000
Control Systems Application Technique
, publication LOGIX-AT001.
Connection
Sets the Connection Type or the Communication Format.
Data Format
Specify the type of data transferred between the device and controller.
Input Data / Output Data
Select the input or output data type for the device.
Counters
Select the counter number for the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal