Device Definition view

How do I open the Device Definition view?
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , double-click the controller to open the device profile.
  3. In the device profile, select
    Device definition
    .
Use
Device Definition
to:
  • View the device type.
  • Configure device-specific settings.
    TIP:
    The parameters are based on the device being configured. The parameters that do not apply to the device are hidden.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal