Channels view (input devices)

Use the
Channels
view to:
  • Enable HART
  • Scale the signal to engineering units
  • Select the input type and range value
  • Configure filters
  • Configure Real Time Sample times
  • Configure the time to keep HART replies
  • If supported, configure HART pass through
  • If supported, disable alarms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal