Port Configuration view parameters (multiple ports)
The
Port Configuration
view (multiple ports) includes these parameters:
TIP:
The parameters that you can view in the
Port Configuration
view are dependent upon the specific device in use.The options appear shaded when the device is a controller. In addition, the options appear shaded and have no value when the device is:
- Offline.
- Online and a communication error occurs.
- Online and theEnablecheckbox is cleared.
- Online and theLink StatusisInactive.
Parameter | Description |
|---|---|
Module | Indicates the device to which this configuration applies. |
Port | Displays the port number. |
Enable | Select or clear the checkbox to enable or disable the port. |
Link Status | Displays the status of the port communication on the network. |
Auto-Negotiate | Indicates that the device automatically selects the best method for communication. If cleared, the port speed and duplex must be set manually. |
Speed - Selected | Specifies the configured port speed for sending and receiving data. Available options are device dependent. Tip : Selected Speed is unavailable if Auto-Negotiate is selected. |
Speed - Current | Displays the actual speed at which the port is currently sending and receiving data. |
Duplex - Selected | Specifies the configured port duplex setting:
Tip : Selected Duplex is unavailable if Auto-Negotiate is selected. |
Duplex - Current | Displays the actual duplex method that the port is currently using to send and receive data. |
Port Diagnostics | Opens Port Diagnostics to view the interface and media counters for the port. |
Enable USB | Enables the USB port. |
Refresh | Retrieves and displays the latest information from the device. |
Set | Writes pending edits to the device. |
Reset | Initiates a reset operation on the device, which returns the device to its power-up state by emulating the cycling of power and causes the changes made to become the port’s current settings. |
Provide Feedback