Configure the port settings

Use the
Port Configuration
view to configure the port settings for non-controller devices.
Prerequisites
  • You must be online and communicating with the device.
  • Ensure a connection interruption at this time is acceptable.
    IMPORTANT:
    Configuring the port settings requires data to be written to the device, which interrupts the connection to the device and to any other device that is connected through it. Connections from other controllers may be interrupted as well. You must not interrupt the connection on a device that is currently being used for control.
To configure the port settings
  1. On the tab for the device, select
    Port Configuration
    .
  2. In the
    Port Configuration
    view, configure the settings as needed.
  3. Select
    Set
    to write the changes to the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal