Configure advanced network properties for bridge devices

Use
Advanced Network Configuration
to configure advanced network properties.
For more information on how to configure the advanced network properties, refer to EtherNet/IP Embedded Switch Technology Application Guide (Publication ENET-AP005).
To configure advanced network properties for bridge devices
  1. On the tab for the device, select
    Network
    .
  2. In the
    Network
    view, select
    Advanced
    .
  3. In
    Advanced Network Configuration
    , configure the network properties as needed.
  4. Select
    Set
    to write the changes to the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal