Advanced Network Configuration parameters
Advanced Network Configuration
includes these parameters.The information is only available when the application is online, and there is no communication error in the device profile.
Parameter | Description |
|---|---|
Network mode | Shows that the device profile is online to a Device Level Ring (DLR) capable device. |
Network topology | Displays the current network topology as either:
Network topology has no value when:
|
Supervisor precedence | Displays the device’s supervisor precedence or enter a value for the supervisor precedence that is in the range of 0…255. Supervisor precedence appears shaded when:
|
Active ring supervisor | If the network is operating in a Ring mode, displays the IP Address or MAC Address of the active ring supervisor. Active ring supervisor appears shaded when:
|
Active supervisor precedence | If the network is operating in a Ring mode, displays the active ring supervisor’s precedence. Active supervisor precedence appears shaded when:
|
Supervisor status | When the device is configured as a supervisor, displays the device’s supervisor status as:
Supervisor status appears shaded when:
|
Supervisor mode | Display the device’s supervisor mode on the network as either:
Supervisor mode has no value when:
|
Ring Parameters |
|
Set | Select Set to commit your modifications.Set appears shaded when:
If ring parameters are changed, the changes only take effect if the device is the Active Ring Supervisor after committing your modifications. |
Provide Feedback