Disable IP settings set by switches on the device

When using the switches on the device to set the IP address,
IP settings set by switches on the device
is set automatically.
To disable IP settings set by switches on the device
  1. Change the switch settings on the device.
  2. Reset the device by either of these two ways:
    • Cycling power to the device.
    • Selecting
      Reset Device
      in the
      Device Information
      view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal