Gateway address

A gateway connects individual physical networks into a system of networks. When a node needs to communicate with a node on another network, a gateway transfers the data between the two networks. This figure shows gateway G connecting Network 1 with Network 2.
1756enetex2
When host B with IP address 128.2.0.1 communicates with host C, it knows from C's IP address that C is on the same network. In an Ethernet environment, B then resolve C's IP address to a MAC address (via ARP) and communicate with C directly.
When host B communicates with host A, host B knows from A's IP address that A is on another network (the net IDs are different). In order to send data to A, B must have the IP address of the gateway connecting the two networks. In this example, the gateway's IP address on Network 2 is 128.2.0.3.
The gateway has two IP addresses (128.1.0.2 and 128.2.0.3). The first must be used by hosts on Network 1 and the second must be used by hosts on Network 2. To be usable, a host's gateway must be addressed using a net ID matching its own.
This field is set to 0.0.0.0 by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal