Domain name

Valid characters consist of:
  • Numbers in the range of 0…9
  • Alpha characters in the range of A…Z (upper or lower case)
  • dash
  • period
  • No more than 48 valid ASCII characters
  • The first and last character of the Domain Name cannot be a period or a dash
  • The last portion of the Domain Name can contain only alpha characters
  • The Domain Name cannot contain two periods next to each other
The valid format for the domain name is:
  • a.b.c.d
  • a.b.c
  • a.b
  • a
For example, these are legal domain names:
  • xyz.xxx.yyy.com
  • 123.xxx.yyy.com
  • 123.123.123.com
  • 123.123.com
These are illegal domain name examples:
  • 123.345.789.123
  • 1234567890
  • 123.
  • .467
  • 123..com
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal