Device Information view parameters
The
Device Information
view includes these parameters.
TIP:
No online data is shown when the device is being created or in the offline mode. The parameters and values are based on the device being configured. The parameters and values that do not apply to the device are hidden.
Parameter | Description |
---|---|
Identification | Displays information that identifies the device:
|
Status - Major/Minor fault | Displays whether there is a major and minor fault. For a digital device, these values are available:
For an analog device, these values are available:
For other devices, these values are available:
|
Status - Internal state | Displays the device's current operational state. Possible values include:
Tip : If the wrong device is selected from Add device , a hexadecimal value is displayed. A textual description of this state is only given when the provided device identity is a match with the actual device. |
Status - Configured | Displays Yes or No indicating whether the device was configured by the owner controller connected to it.Once a device is configured, it stays configured until the device is reset or power is cycled, even if the owner drops connection to the device. This applies only to I/O devices and does not apply to adapters, scanners, bridges, or other communication devices. |
Status - Owned | Displays Yes or No indicating whether an owner controller is currently connected to the device.This applies only to I/O devices and does not apply to adapters, scanners, bridges, or other communication devices. |
Status - Device identity | Displays whether the physical device matches or mismatches with the configuration in the Overview view.
Tip : Device identity does not take into account the Electronic keying or Minor revision settings in the Overview view. The Generic devices, such as the 1756 devices, always show a Mismatch because the configured Generic Key does not match any target device. |
Timer Hardware (when enabled) | Displays whether the timer's hardware is OK or Faulted . |
Timer Sync'ed (when enabled) | Displays Yes or No indicating whether the device's time is coordinated with the master. |
Status - Protection mode | Displays the device protection when online. The protection mode depends on the device and may include:
Tip : When the device is offline or if a communication failure to the device occurs, the field is blank. |
Diagnostics | Opens Device Diagnostics for diagnostic information. |
Reset Device | Initiates a reset operation on the device, which returns the device to its power-up state by emulating the cycling of power. IMPORTANT : Resetting a device closes all connections to or through the device, which may result in loss of control.Tip :
|
Reset Module A | (Duplex devices only) Initiates a reset operation on Module A of the device, which returns Module A of the device to its power-up state by emulating the cycling of power. IMPORTANT : Resetting a device closes all connections to or through the device, which may result in loss of control.Tip :
|
Reset Module B | (Duplex devices only) Initiates a reset operation on Module B of the device, which returns Module B of the device to its power-up state by emulating the cycling of power. IMPORTANT : Resetting a device closes all connections to or through the device, which may result in loss of control.Tip :
|
Refresh | Retrieves and displays the latest values from the device. |
Provide Feedback