Device Information view

Use the
Device Information
view to view device and status information when the device is online.
Use the
Device Information
view to:
  • Determine the identity of the device.
  • View the device's current operational state.
  • View whether the device was configured by the owner controller.
  • View whether an owner controller is currently connected to the device.
  • Retrieve the latest information from the device.
  • Reset a device to its power-up state.
  • If supported, view the protection mode of the device.
TIP:
The data in the
Device Information
view comes directly from the device. The
Device Information
view might not be available when the connection is set to Listen Only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal