Eventxx View
The Eventxx view, where 'xx' represents the index of an event definition, shows the
configuration options available for that event. You cannot configure the parameters from
this view, you must use the configuration tags.
Use this view to review the following tasks:
- Whether the event is enabled.
- Whether the event is latched.
- Whether independent point triggers for the event is enabled.
- Check the trigger condition for the event.
- Check the participants and their State Transition behavior for the event.
Eventxx View Example

The Eventxx view includes these parameters.
Parameter | Description | Member Name | Value |
|---|---|---|---|
Enable Event | Displays whether the corresponding event trigger is active. Events
are triggered when conditions match the event definition. | EO.Eventxx.En |
|
Latch Event | Displays whether an event is latched until it is acknowledged. | EO.Eventxx.LatchEvent |
|
Enable Independent Point Triggers | Displays whether each condition indicated in the Event trigger
definition can initiate an event independently. | EO.Eventxx. IndependentConditionTriggerEn |
|
Trigger Event | Triggers an event each time a state change results in one of the
following conditions:
|
| Values (EventRisingEn, EventFallingEn) represent:
|
Event Trigger Pattern – Participate in Event Trigger | Displays whether the specified condition participates in the Event
trigger definition for the event. | When Encoder Type is configured as HSC:
When Encoder Type is configured as SSI:
|
|
Event Trigger Pattern – State Transition | Displays the state of the condition to match after the
transition. | When Encoder Type is configured as HSC:
When Encoder Type is configured as SSI:
| For InWindowxxValue:
For other event tags:
|
Provide Feedback