Update an EDD file for a specific HART device

  1. From the Module Properties dialog - General view, select Change...
  2. From the Module Definition dialog, select Add HART EDD...
  3. In the Add HART EDD dialog box, browse to the location of the EDD file.
  4. Select the HART EDD file and select Open.
    The message Successfully added EDD appears.
  5. Select OK to close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal