Add HART EDD File
There are two scenarios for adding HART devices from the Module Definition dialog box:
- Update an EDD file for a specific HART device.
- Add an EDD file for a generic HART device.
The HART device EDD files are included with most HART device profiles. If additional or
newer EDD files are required, download the EDD file. This file may be available from the
Documents and Downloads page at the FieldComm Group website www.fieldcommgroup.org. Otherwise request the file from the HART Device
vendor.
Provide Feedback