Replace a Device with ADC Disabled and DS Not Supported or Disabled

Verify that you have completed the procedure as described in Prerequisite Steps.
To replace a device in this scenario, complete these steps.
  1. Replace the physical device.
  2. Go online with your project.
  3. In the IO-Link device Module Properties → Configuration view, perform Device Correlation Check and select “Use Project Values” to download the configuration to the replacement device.
    If the device configuration that is saved in the project is outdated, you must manually configure the replacement device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal