Prerequisite Steps

To help ensure that replacing an IO-Link device is successful in the following scenarios, first back up the device configuration to the project in advance by completing these steps.
  1. While the old device is attached to the port of the IO-Link master module, go online with your project.
  2. In the IO-Link device Module Properties > Configuration view, perform Device Correlation Check.
  3. If there are differences, select “Use Device Values” to back up the device configuration to the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal