Summary of Changes

This publication contains the following new or updated information. This list includes substantive updates only and is not intended to reflect all changes. Translated versions are not always available for each revision.
Summary of Changes
Topic
Page
Updated terminology table.
Updated Additional Resources.
Added 5034-IA8/XT and 5034-OA4/XT module details.
Added important note for 5034-IA8/XT module.
Updated Triggered Pulse Output.
Added Surge Suppressors for Relay Output Modules.
This publication contains the following new or updated information. This list includes substantive updates only and is not intended to reflect all changes. Translated versions are not always available for each revision.
This publication contains the following new or updated information. This list includes substantive updates only and is not intended to reflect all changes. Translated versions are not always available for each revision.
This publication contains the following new or updated information. This list includes substantive updates only and is not intended to reflect all changes. Translated versions are not always available for each revision.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal