Field Power Loss Detection

Field Power Loss Detection for SA Power

IMPORTANT:
All digital output modules support SA power except 5034-OA4/XT module.
The Field Power Loss Detection feature monitors for the loss of field-side power on the SA power bus.
In the diagnostic assembly, the FieldPowerOff bit is set at the module and point level structure. The Fault bit is set at the point level.

Field Power Loss Detection for LA Power

IMPORTANT:
The 5034-OA4/XT module supports LA power only when the module operates in AC mode.
The Field Power Loss Detection feature monitors for the loss of field-side power at the LA power terminal on the RTB.
In the diagnostic assembly, the FieldPowerOff bit is set at the module and point level structure. The Fault bit is set at the point level.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal