Add the HART EDD file
The HART device EDD files are included with the HART device profiles. If additional EDD
files are required, download the EDD file. This file may be available from the Documents
and Downloads page at the FieldCommGroup website https://www.fieldcommgroup.org. Otherwise
request the file from the HART Device vendor.
To add the HART EDD file
- From theDevice definitiondialog box -Overviewview, selectAdd HART EDD.
- In theAdd HART EDDdialog box, browse to the location of the EDD file.
- Select the HART EDD file and selectADD.The messageSuccessfully added EDDappears and the dialog box closes.
When adding a HART EDD file, an error message appears when:
- the selected file is not an EDD file.
- an EDD file for the device is not included.
- the device revision is not found for the device.
Provide Feedback