- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Dropdown button
Button that opens/closes a pop-up panel when selected
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Panel | Panel | Panel to be displayed. Must be a widget | |
Panel alias node | PanelAliasNode | Node to which to point any alias in the panel to be displayed | |
Animation | AnimationType | Type of opening/closing animation | |
Close on click inside | CloseOnClickInside | Close the pop-up panel when selecting inside its area | |
Close on click outside | CloseOnClickOutside | Close the pop-up panel when clicking outside its area | |
Direction | Direction | Direction of opening/closing of the panel, horizontal or vertical | |
Style | Style | Graphic style applied to the control | |
Text | Text | (Inherited from Button) | |
Appearance | Appearance | (Inherited from Button) | |
Image path | ImagePath | (Inherited from Button) | |
Image position | ImagePosition | (Inherited from Button) | |
Text position | TextPosition | (Inherited from Button) | |
Image width | ImageWidth | (Inherited from Button) | |
Image height | ImageHeight | (Inherited from Button) | |
Word wrap | WordWrap | (Inherited from Button) | |
Text trimming | Elide | (Inherited from Button) | |
Font family | FontFamily | (Inherited from Button) | |
Font weight | FontWeight | (Inherited from Button) | |
Font italic | FontItalic | (Inherited from Button) | |
Font size | FontSize | (Inherited from Button) | |
Text color | TextColor | (Inherited from Button) | |
Background color | BackgroundColor | (Inherited from Button) | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Provide Feedback