Editing storage locations

  1. In either the
    Hierarchy
    or
    Detail
    pane, right-click a storage location, and then select
    Properties
    . The
    Edit Material Storage Location
    dialog opens to the
    General
    tab.
    FTBMM_ED_Storage Location_Edit General tab
  2. Make any necessary changes to the general information, and then click
    Apply
    .
  3. Select the
    Materials
    tab. The materials assigned to this storage location display.
    FTBMM_ED_Storage Location_Edit Materials tab
    To make any changes to the list of configured materials, you need to edit the storage container located in the storage location. (See Editing storage containers for more information.)
  4. To view material properties, double-click a material. The
    View Material
    dialog opens.
    FTBMM_ED_Storage Location_View Materials
    You only can view the material’s property values. To edit the values, use the
    Edit Material
    dialog. (See Creating a material record for more information.)
  5. Click
    Close
    to close the dialog.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal