Editing storage containers

  1. In either the
    Hierarchy
    or
    Detail
    pane, right-click a container, and then select
    Properties
    . The
    Edit Material Storage Container
    dialog opens to the
    General
    tab. The container name displays in the title bar.
  2. Make the necessary changes to the storage container.
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
  3. Click
    OK
    to save the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal