Creating storage locations
Storage locations represent the locations of actual material storage containers. When adding new locations, you must add a record of the location before you can configure it.
- In theHierarchypane, right-clickLocations, and then selectNew Material Storage Location. TheCreate Material Storage Locationdialog opens.

- In theNamebox, type a unique name for the material.
- In theDescriptionbox, type a detailed description of the material.
- In theController IDbox, type a unique number if desired. If left at 0 (zero), theController IDdefaults to the next numeric value in sequence.
- ClickOKto save the new location and close the dialog.
- In either theHierarchyorDetailpane, right-click the storage location, and then selectNew Material Storage Container.
- Configure the material storage containers for this storage location. (See Configuring storage containers for more information.)
Provide Feedback