Editing states

  1. From the
    States Configuration
    dialog, select the
    Lot
    or
    Container
    tab.
  2. Select the record row to edit, and then click the
    Edit State
    button. The
    Edit Lot
    (or
    Container
    )
    State
    dialog opens.
  3. Make the necessary changes, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal