Configuring states

The state of a lot informs others about the availability of a material. When a lot of material is assigned the state of
Ready To Use
, it can be distributed to its configured containers and used in a recipe. You can use lot states to keep certain lots of material from being used in a recipe. For instance, you can assign a
Rejected
state to a material that does not conform to standards. Since the state is not
Ready To Use
, the
FactoryTalk Batch
Server does not use the material.
The same rule applies to the state of a container. If a container is not
Ready To Use
, you cannot distribute material to that container, either as an addition of material from a container to a recipe, or the distribution of material to a container from the recipe. You can use container states to keep certain containers from being used. For example, when a container needs a maintenance check, assign the
Maintenance
state. Since the state is not
Ready To Use
, the
FactoryTalk Batch
Server does not use the container.
The
States Configuration
option allows you to pre-configure descriptive information about the lot and container states, but not report an actual quantity of that lot or container.
TIP:
The
FactoryTalk Batch
Server can bind a recipe only to a material or container that is
Ready To Use
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal