Configure material inventory

The
Inventory
tab displays a view of the material lot distribution. Each row represents a sublot. A sublot is an amount of material in the selected lot that is distributed to a container. The container, lot, and label are used by the
FactoryTalk Batch
Server when searching for a material to bind to a recipe. When the recipe is complete, the
FactoryTalk
Batch Server updates the amount to reflect the amount of material either consumed from the container (Addition) or added to the container (Distribution). You configure the container type in the
FactoryTalk Batch
Equipment Editor. [See the for more information.]
When you edit, distribute, or delete a distribution in a material’s inventory, the results also affect the container’s inventory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal