Using a form to edit material class properties
- On thePropertiestab, select the record row to edit, and then click theEdit Propertybutton. TheEdit Material Class Propertydialog opens.

- Make the desired changes. You cannot change theType.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- If you want to propagate the changes to all material and lot properties that are based on this material class, selectSynchronize.
- ClickOK.
Provide Feedback