Edit material class properties
Use this procedure to edit material class properties.
To edit material class properties:
- If you need to change the material class properties, select thePropertiestab from theEdit Material Classdialog. The currently defined material class properties display in a table format. You can also use a form to make changes. SeeUsing a form to edit material class propertiesfor more information.

- Make the desired changes. You cannot change theType.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value containing a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- If you want to propagate the changes to all material and lot properties that are based on this material class, selectSynchronize.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog.
Provide Feedback