Install OSIsoft AF Client
To connect InfoPlatform with Historian, install the following:
- To install the OSIsoft’s AFClient, run the setup from the media as specified in the section: “InfoPlatform Service Installation Package”
- Refer to OSIsoft documentation for additional information.
Provide Feedback